Browse FAQs

What is the maximum number of PDO's that you can put in a Twido CANopen Master TWDNCO1M?

Published date: 07 February 2019

Issue:
Max number of PDO for the Twido.

Product line:
Twido

Environment:
TwidoSuite, TwidoSoft

Resolution:
The RPDO or TPDO is a 64-byte object that can contain up to eight 8-byte word objects or four 16-byte word objects or any combination of those two types of word objects, not too exceed the overall 64-byte limit of the PDO.
To customize the PDO mapping, select the Mapped Object you wish to modify.
Note: You can not add a 32 byte object into the PDO.

NOTE: The Twido is obsolete 12/31/2016 and has ben replaced with the M221 and the M221 does not support CANopen.
 
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.