Search FAQs
What are the Contact Resistance values for the Evolis 24KV Circuit Breaker.
The contact resistance values for the Evolis 24KV Circuit Breaker are tabulated below :
Evolis 24KV | 16kA -630A | 25kA-1250A | 31.5kA-2500A | ||||
Fixed | Withdrawable | Fixed | Withdrawable | Fixed | Withdrawable | ||
Contact Resistance | current supplied : I = 100 A | < 55 µΩ | < 80 µΩ | < 45 µΩ | < 70 µΩ | < 30 µΩ | < 35 µΩ |
Released for:Schneider Electric United Arab Emirates
Explore more
Range:
Explore more
Range: