Technical FAQs

Ask a Question

What does the parameter uLu mean in the ATV212 programming?

Issue:
What  does the parameter uLu mean in the ATV212 programming?

Product Line:
Altivar ATV21, ATV212

Environment:
All

Cause:
N/A

Resolution:
ULU is the motor voltage parameter.  It is programmed to match the motor voltage.  

Was this helpful?
What can we do to improve the information ?