{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Can I connect to a SoMachine controller using the bluetooth adapter TCSWAAC13FB?


This is possible with SoMacihne V4.3.

gateway
Due to the fact that HMISCU COM (RJ45 connector) pin 7 does not provide power to the connected device it won’t work with the SCU. The other controllers provide 5V to this pin so that the adapter is powered.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.