Browse FAQs

How can we connect the charging station to solar panels?

Published date: 12 February 2019

Solar panels generate DC current so this energy cannot be directly used to supply charging stations. It is required to install a DC/AC inverter. Additionally, if the energy generated by the solar panel is not enough to supply the charging station full time, another energy source is required and a switching station behind the solar inverter must be installed to switch sources when the solar panels are not able to sustain the demand. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.