Welcome the the Schneider Electric French website.
It looks like you are located in the United States, would you like to change your location?
Traduisez en francais
Browse FAQs
what is the meaning of "Use Manual Setup" Error screen in Power Factor Regulator NRC12 ?
Published date:
12 March 2021
As per page # 20 of the attached Varlogic NRC12 User Manual, the "Use Manual Setup" error message is generated when a non-relevant information result from the auto-setup process. And the solution in this case would be for the user to perform manual setup to confirm or correct the information obtained by auto-setup.