Browse FAQs

What is the maximum number of Insulation fault locators IFL12 that can be connected to IM400?

Published date: 15 March 2021

Please note that with the vigilohm IM400 you can associate unlimited number of Insulation Fault Locators IFL12 because there is no wired connection  needed between the Insulation Monitor and the Insulation Fault Locators.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.