{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

Choose another country or region

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

What is the Easergy flair VD23(voltage detection relay) Power consumption details which is not available in the manual?

Issue:
Power consumption value for Easergy flair VD23

Environment/Product line:
Easergy flair VD23 relays

Resolution :
Average consumption of the VD23 is less than 30 mA.

During switching operation of internal relays, peak consumption can increase up to 60 mA for 20 ms max.

Consumption values are applicable on full input voltage range of the V23.
 
Explore more

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.
Explore more