Browse FAQs

For Easergy T300, Can VPIS VO V3 be used with SC150 for power measurements and power quality?

Published date: 15 January 2021

Issue:
need to get power measurements and power quality while using VPIS VO V3 with SC150

Environment:
Easergy T300 

Resolution:

- If VPIS VO V3 is being used with SC150-CT-LPVT/VT; then power measurements and power quality are available (with low accuracy).
- If VPIS VO V3 is being used with SC150-CT-CAPA; then no power measurements or power quality will be available.
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.