Technical FAQs

Ask a Question

Is the VW3A1111 keypad compatible for use with the ATV320 drives?
Issue: Is the VW3A1111 keypad compatible for use with the ATV320 drives? Product Line: ATV320  Environment: All serial numbers Cause: Revision to...
Is it possible to compare or convert configurations from ATV61/71 to ATV6xx in SoMove?
Issue:   Can you compare or convert configurations from ATV61/71 to ATV6xx in SoMove? Product Line: Altivar 61, Altivar 71 , Altivar 630, Altivar...
Is the ATV630 process drive compatible with the Multiloader tool?
Issue: Is the ATV630 process drive compatible with the Multiloader tool? Product Line: Altivar Process, ATV630 Environment: All Cause: N/A Resolution:...
Can the existing Full Function Test Kit (FFTK) be used for testing the new Compact NSX MCCB?
Compact NSX can be tested with a new dedicated test kit, Maintenance case reference TRV00910. This TRV00910 test kit works in association with the...
Why is it not possible to have a built in motor mechanism for Compact NS630 LB and NS800 LB Circuit Breakers.
The basic frames of the Compact NS630b LB and NS800 LB Circuit Breakers have been modified as compared to the basic frame for the other Circuit Breakers...
Is the installation of 31097 locking kit same as the 31088 in Interpact source changeover system.
Yes, the installation of the 31097 & 31088 locking kits is the same, as all key locks have been designed to achieve locking in the OFF position. Refer...
What are the characteristics of SR13MAE (MAE500) trip unit used in Compact NS630 circuit breaker.
The Compact NS630 fitted with the STR13MAE trip unit is named: NS630MAE500.   The old MA500 trip unit was designed with mechanical feature. The new...
Is the HMIGTU 12' display (HMIDT643) with built in WIFI compatible with both HMIG3U and HMIG5U?
Issue: It is not possible to select the HMIDT643 with built in Wifi for a HMIG3U in Vijeo Designer or Vijeo XD. Product Line: HMIG3U, HMIG5U, HMIDT643...
Will the B882-239 High Speed Counter support a quadrature input ?
No, the B882-239 does not support quadrature mode. You would have to use the B883-001 HSC for a quadrature operation. Legacy KB System (APS) Data:...
What is the minimum screen resolution to be used with Concept 2.6?
The minimum screen display resolution for Concept 2.6 is 800 x 600 pixels. 
Results 1 - 10 of 93