{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

How to to unlock the drive using master reset password for ATV310 ?

1. Go to the 999. Press Enter. ON will be displayed ( meaning drive is password protected and hence access to FULL menu and factory reset is not permissible) 2. Rotate jog dial clockwise and set...

how can i access ATV 61 VFD by web server it is asking user name and...

Please check the Standard webserver section in all the attached documents, Generally, By default, the user name and the password (HTTP password) are both “USER” (upper case)

What is the function of the Unika Sockets with interlock switch ?

In conformity with IEC 60309 standards, all the industrial sockets have a lock or holding mechanism, which keeps the plug firmly locked in the socket, preventing it from being pulled out...

What is replacement of eocrss-30s ?

kindly be informed that EOCR is under Samwha which is not locally offered and this range in commercilaized only in South Korea. However, kindly find attached the commercialized in Schneider product...

What is the BOM of MVS25H4MW6A ?

The reference MVS25H4MW6A consists of the following:- MVS22154 MVS25H_4PW_SA MVS21418 ETA 6G - Drawout 48169 TOP 4P HORIZ. REAR CONNECTION 48174 BOTTOM 4P HORIZ. REAR CONNECTI

What is the BOM of MVS25H4MF5L ?

The reference MVS25H4MF5L consists of the following:- 48169 TOP 4P HORIZ. REAR CONNECTION 48174 BOTTOM 4P HORIZ. REAR CONNECTI MVS21424 ET 5S FIXED MVS22162 ADAPT EP MVS 2500A H

How to read all the fault records in Micom P111 relay?

All the fault records can be read from this address single address 01 03 37 00 00 0E CRC . If you need the serpate address /mapping details ,please visit our below website to download the manual to...

What are the different license sizes of Unity Pro 11 ?

Unity Pro V11 is available in 3 different sizes : S, L, XL The only difference between sizes S, L, XL is the supported controller references. Supported PLCs by size :

Popular Video FAQsPopular Videos

video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail
video-thumbnail

Learn more through our Generic Knowledge FAQsGeneral Knowledge

How to reset Zelio logic password?

The password can be reset by clearing the program inside the Zelio either by Transfering a new program to the Zelio Or Clearing the program that already exist by updating the firmware Kindly find the...

What is meant by Symmetrical and Asymmetrical breaking currents?

issue: Customer wants to know the value of the symmetrical and asymmetrical breaking current of the circuit breaker and what do they mean. Environment: Circuit Breaker Resolution: - Symmetrical...

Why are some products double coded with two IP ratings (like IP65 / IP67)?

The second characteristic numeral in an IP designation indicates the degree of protection provided by enclosures with respect to harmful effects on the equipment due to the ingress of water. 5 =>...

Can I install bypass contactor for Altivar process drives?

Bypass contactors are not supported by ATV process LV drives (ATV600, ATV900). It is not possible to bypass the drive by external contactors because there is no synchronization of output voltage with...

In a 3 phase system, why does the meter still show voltage reading on one...

Issue: Testing phase loss on a meter doesn't result in a null voltage reading. Environmnet: EasyLogic Series Power Meters PowerLogic Series Power Meters Resolution: The voltage seen is what we...