Technical FAQs

Ask a Question

Filter results

Clear
What are the Share-UPS and Interface Expander modes of operation?
Issue What are the Share-UPS and Interface Expander modes of operation? Product Line   UPS Device Management AP9607/AP9607CB Interface Expander SmartSlot...
How do you update the M241 or M251 firmware using SoMachine Controller Assistant?
Issue How do you update the M241 or M251 firmware using SoMachine Controller Assistant? Product Line Modicon M241 PLC Modicon M251 PLC EcoStruxure...
Which communication protocol is used between a Compact NSX and display FDM121.
The communication protocol used between the Compact NSX and FDM121 display is Universal Logic Plug (ULP). This a Schneider Electric internal protocol.
Where to download M580 Firmware?
Issue: Where to download M580 Firmware? Product Line: M580 Resolution: The M580 Firmware can be downloaded from here: https://www.schneider-electric.ca/en/download/range/62098-Modicon%20M580%20High-end%20Controller/?docTypeGroup=88181372-Software%2FFirmware...
Why does my USB drive show up as a Modicon PLC in the Device Manager?
 Issue: USB drive does not work properly and shows up as a Modicon PLC in the Device Manager of the PC.   Product Line: Modicon PLC   Environment:...
How to install the USB driver for Zelio Soft2 and install USB cable SR2USB01.
Follow the step by step procedure in order to install the USB driver for Zelio Soft2 and the USB cable SR2USB01 for two different operating systems...
What are the part number and driver for the serial port (9-Pin D-Shell) to USB converter for Modicon Quantum PLC.
The part no. of the Schneider USB to RS232 Converter is TSXCUSB232 Refer the attachment for the TSXUSB232 documentation.   Use the standard Schneider...
Where can I download SoMove and DTM files? What is the USB to RJ45 cable required to connect SoMove to the drive using the ModBus port?
Issue: Where can I find a link for SoMove? What cable is used? Product line: Variable Frequency Drives and Soft Starts   Environment: All models,...
I have the TCSMCNAM3M002P USB to RS485 converter cable, how can I download the drivers to use it?
For TCSMCNAM3M002P cable TSXCUSB and TCSMCNAM DRIVER need to be installed  The drivers can be downloaded from below link : https://www.schneider-electric.com/en/download/document/TSXCUSB+and+TCSMCNAM+DRIVER/...
How to calculate the scan time of Hot Stand-By (HSBY) system in Modicon Quantum range.
Considering the Hot Stand-By system, the scan time mainly comes from the addition of three parts:   Part 1: User application logic execution time,...
Results 1 - 10 of 44