Technical FAQs

Ask a Question

Filter results

Clear
Preventa XY2C_How to order the commercial reference XY2CH13150H7 in 2019? is it available to order?
Please note that the XY2CH13150H7 commercial reference is available to order in 2019, under internal logistic reference XY2CH13150H7AC. Please contact...
How can I tell if my ATV61 or ATV71 drive is in sleep mode? (Low speed timeout active).
Issue: How can I tell if my ATV61 or ATV71 drive is in sleep mode? (Low speed timeout active). Product Line: ATV61 / ATV71 series drives. Environment:...
8839 EFD... is an invalid part #. Also 8839 MFD... 8839 SFD... 8638 48U... 8639 48U... 8639 22U...8839 CPD... 8930 IFD... SFD212...
Issue:  The part number does not come up as a good part number in Q2C. Product Line:   EFlex, MFlex, SFlex with non-standard Mods, Enclosed Drives,...
What is the Export Control Classification Number (ECCN)? Is it applicable for Mcset range?
An Export Control Classification Number (ECCN) is an alphanumeric designation (i.e., 1A984 or 4A001) used in the CCL (commerce control list) to identify...
What is the Export Control Classification Number (ECCN)? Is it applicable for PIX range?
An Export Control Classification Number (ECCN) is an alphanumeric designation (i.e., 1A984 or 4A001) used in the CCL (commerce control list) to identify...
INFORMATION BULLETIN - Using Global Outlet Groups simultaneously between AP79XX and AP8XXX series Rack PDUs with the same multicast IP range causes AP79XX PDU not to boot properly
Issue An issue has been identified with AP79XX series Switched Rack PDU users who enable the global outlet group functionality. If the user has AP79XX...
Results 1 - 6 of 6
  • 1