Technical FAQs

Ask a Question

I already have a serial number for Schneider Electric Automation and HMI programming software, where can I download it?
Issue Where to download programming software Product line Ecostruxure Control Expert, ProWORX 32, Concept, SoMachine and Vijeo Designer Resolution...
Why can I not enable the Implicit Type Conversion feature in Unity Pro V8.0?
Issue Enable Implicit Type Conversion Product Line Unity Pro  Control Expert Resolution The Enable Implicit Type Conversion feature was not available...
Is it possible to change the root directory of web visualization in SoMachine?
Issue: Is it possible to change the root directory of a web visualization? The default is /usr/visu/, but I would like to put it on the removeable...
Connect a remote OPC client to ClearSCADA
Problem Need to connect a remote OPC client to ClearSCADA and bypass DCOM. Solution This can be achieved by installing the Data Access component of...
Change default WebX ports in ClearSCADA
This article explains how the default WebX ports can be changed for the redesigned WebX interface in ClearSCADA 2015 R1 and later versions. The default...
What is the replacement for the XBTGT7340?
Issue: What is the replacement for the XBTGT7340? Product Line: Magelis HMI, XBTGT7000 series Resolution: The replacement for the XBTGT7340 is the:...
Can I use the PCFL_AIN block with M340 analog IO?
Yes, you can use the PCFL_AIN block with M340 analog IO. However, you will experience better resolution and scaling capability by using the BMXAMx...
Connect and change parameters on a LXM32 drive using SoMachine
Issue: Can I connect and change parameters on LXM32 servo drive using SoMachine? Product Line: SoMachine Resolution: In SoMachine, when you add a...
Why am I having issues connecting SoMove to an Altivar Drive or Altistart Soft Starter?
Issue: SoMove Troubleshooting:Cannot Connect to SoMove using an Altivar Drive  Product Line: Altivar Drive (ATV61, ATV71) Altivar Machine Drive (ATV12,...
How do I unlock the SQL library in SoMachine v4.2?
Issue: How do I unlock SQL library in SoMachine? Product Line: SoMachine Resolution: Please see attached SQL license activation and installation document...
Results 1 - 10 of 96