Technical FAQs

Ask a Question

Is the braking transistor inbuilt in Altivar 71 Drives?
The Braking transistor is inbuilt in maximum ratings of Altivar 71 Drive. The following Altivar 71 Drive ranges ATV71HpppM3, ATV71HpppM3X, ATV71H075N4…HC16N4,...
Osisense XC_XCMN211AL1 switch datasheet
XCMN211AL1 basic limit switch is not a standard one (not shown into Osisense XC catalogue). It is an adapted switch requested by an Italian OEM. It...
Osisense XC - Oxygen index of the plastic material used in the enclosure of the XCKP, XCMN, XCKT & XCKS limit switches
The plastic case of the XCKP, XCKT, XCMN and XCKS blue limit switches is a blue Valox 553, or PBT+PC GF30. It is flame classified UL94 V-0. Oxygen...
9013FSG - Meaning of the form Z22 in the 9013FSG, FRG, FHG pressure switch references
The form Z22 in the 9013FSG, FRG, FHG pressure switch references, means black cover instead of grey cover.
Can the ATV212 drive run a synchronous motor?
Issue: Can the ATV212 drive run a synchronous motor? Product Line: ATV212 Environment: All serial numbers for ATV212 Cause: N/A Resolution: Yes the...
Osisense XU_XUZCR0501AF anti fog reflector datasheet
Please find attached the datasheet of the XUZCR0501AF anti fog (or anti mist) reflector 51 x 69 mm, which is not a standard reflector.
What is meant by Thermal image in Compact NSX?
The model representing the conductor heat rise is constructed according to the calculation of a thermal image. It allows the thermal state of the...
What is meant by Load profile in Compact NSX.
The load profile is stored in a counter. The counter counts up the number of of operating hours per load section. Example: One counter indicates the...
What is the maximum allowable test voltage and time that can be applied to the Compact NSX MCCB during Dielectric Test.
The Compact NSX Moulded Case Circuit Breaker (MCCB) is tested at the following voltage and time during Dielectric Tests.      For NSX100-250, the...
Which are the materials used in Compact NSX connection terminals.
The material used in the Compact NSX terminal connectors is as below:   Compact NSX100-250 : Copper (Cu) + Tin coating   Compact NSX 400-630: Copper...
Results 1 - 10 of 100