Technical FAQs

Ask a Question

When connected to the wall, my Back-UPS product will not power on.
Issue: When connected to the wall, my Back-UPS product will not power on. * There are many possible scenarios in which a Back-UPS product will not...
The use of non computer type loads with a UPS, specific to Back-UPS, Smart-UPS SC
Issue: The use of non computer type loads with a UPS, specific to Back-UPS, Smart-UPS SC. Product Line: Back-UPS, Back-UPS Pro, Smart-UPS SC Environment:...
Trio Q Series - Bandwidth Challenges
It is important to ensure clarity about the bandwidth capabilities of the Trio Q Series data radio. There are significant challenges with trying to...
How do I Create multiple containers for a multi-monitor setup?
ClearSCADA versions prior to version 2014 R1 allowed multiple ViewX instances to be created on the same client PC for use with multiple monitor set-ups. ...
ClearSCADA Database Backup
Problem How do I properly backup a ClearSCADA database including all history and events? Solution 1 ClearSCADA 2015 and newer features a 'Backup'...
ClearSCADA Database Restore
Problem How do I properly restore a ClearSCADA database? Solution 1 ClearSCADA 2015 and newer features a 'Backup' object.  If a 'Backup' object was...
What is meant by Thermal image in Compact NSX?
The model representing the conductor heat rise is constructed according to the calculation of a thermal image. It allows the thermal state of the...
What is the maximum allowable test voltage and time that can be applied to the Compact NSX MCCB during Dielectric Test.
The Compact NSX Moulded Case Circuit Breaker (MCCB) is tested at the following voltage and time during Dielectric Tests.      For NSX100-250, the...
Will there be any problem if the MX coil (shunt trip) of NS100 to NS630 is continuously kept powered up.
With the newer design technology there will be absolutely no problems if the MX coil (shunt trip coil) of NS100 to NS630 is continuously kept powered...
Why does the display light of Micrologic 6.2 trip unit of Compact NSX not glow even when the load reading is displayed.
Unlike other range of Micrologic the backlighting or display light of Micrologic 6.2 is not self powered by the primary current.   A separate external...
Results 1 - 10 of 100