Gulf countries and Pakistan
Schneider Electric Gulf Countries and Pakistan Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Choose another country or region
  • Chasing storm by accident while taking sunset photos at North Curl Curl, Australia

    Your electronics, protected

    Find out how to protect your precious electronic equipment from electrical surges during lightning storms.

    Download brochure

Surge protection devices: your best defence

Every day, lightning strikes homes and properties somewhere in the world. Any structure in the path of an electrical storm is at risk. While only lasting for a few microseconds, lightning causes a dangerous voltage surge that can destroy your electronic devices. Installing surge protection devices, SPDs, can reduce or even prevent damage to your valuable possessions.
Default Alternative Text

Surge protection devices

Domae SPD

Description
Surge protection device protects your audio and video electrical equipment (electronics) from lightning and power surge traveling over COAX and data lines.
Surge protection Domae is suitable for residential with protection from surge up to 10kA.
Already integrated with MCB as over current protection and earth cable.
  • Did you know?

    • Every day there are about 8 million lightning strikes globally. 
    • The tallest structure is the most likely point of contact in a lightning strike.
    • Isolated structures on large expanses of flat land are likely to attract lightning strikes.
    • While some structures are more likely to attract a strike, lightning is 100% unpredictable.

    Default Alternative Text
  • Lightning risk worldwide

    Lightning strikes can't be predicted, but some regions of the world are more affected than others. Areas marked violet and pink have the highest stroke density, followed by regions in red, orange, yellow, green and blue.

    Lightning density map

    Destruction of electronics

    A power surge can enter your house either via a direct strike, or indirectly. Direct strikes occur when lightning passes directly through a building, often causing major damage and fires. Indirect strikes occur when lightning strikes ground nearby, or power lines directly connected to a house. When this happens, any connected appliance or electronic device can be destroyed.

    The result:
    • High replacement costs of electronics and circuitry
    • Disruption of your personal and/or professional connectivity
    Default Alternative Text

    Think your equipment is protected?

    Think again. Even if you already have a lightning rod installed, it might not be enough. It can direct a strike around the exterior of a structure, but some overvoltage can still enter the building’s electrical circuitry and damage any electronics that are not protected by SPDs.
    • Lightning pathways

      In a direct lightning strike on a building with no protection, a voltage spike can enter your home through the switchboard and destroy all your electronic equipment.

      Go to the next slide to see more.

      An image of a house where direct lightning strikes on a building with no protection
    • Lightning pathways

      When lightning strikes near a building with no protection, it can travel inside via power lines directly connected to the switchboard.

      Go to the next slide to see more.

      An image of a house when lightning strikes near the building with no protection
    • Lightning pathways

      When lightning strikes a building with a lightning rod, most of the overvoltage is directed to ground around the outside of the building. However up to half the overvoltage can still enter your home via the electrical circuitry.

      Go to the next slide to see more

      An image if a house when lightning strikes a building with a lightning rod
    • Lightning pathways

      When lightning strikes near the building even with protection, it can travel into your home via power lines directly connected to the switchboard.

      An image of a house when lightning strikes near the building even with protection

      Protecting your equipment with surge protection devices

      A lightning strike near a building or overhead supply lines suddenly increases the voltage from 230 V to 3 or 6 kV. The resulting surge, which lasts a few microseconds, can destroy electronic components such as memory, processors, capacitors, and screens.

      An SPD can damp the spike down to a value compatible with that which most connected appliances can withstand: approximately 1.5 kV. All devices within 10 meters of the switchboard are effectively protected. If your devices are more than 10 meters away from the installed SPD, additional protection needs to be added, such as a type 3 SPD in a nearby switchboard of a power strip with integrated surge protection.
      • Default Alternative Text
        Surge Arrester SPDs protect sensitive appliances and electronics by directing energy surges in the supply line straight to the ground. Learn more
      • Default Alternative Text
        Protective power strip Connecting your appliances to a power strip with integrated surge protection will greatly reduce the risk of damage during a lightning strike. Learn more

      How to get support from your electrician

      • Default Alternative Text
        Trust a qualified electrician to advise you of the right Schneider Electric SPDs: Type 1, 2 or 3.
      • Default Alternative Text
        Your electrician can help choose the right SPD rating: 20kA or 40kA, depending on your geography and building type.
      • Default Alternative Text
        For increased protection, your electrician can advise using lightning rods together with SPDs.

      Electrical Installation Wiki

      Learn about voltage surges and overvoltage protection With over 8 million lightning strikes occurring globally every day, it’s crucial to know how to protect your home with surge protection devices.
      Learn more

      Protect your electronic equipment from lightning related damage

      Safeguard your technology from lightning You’ve invested a lot in the technology that makes your family’s lives easier and more enjoyable. Now you need to protect it from lightning strikes.
      Learn more

      The Chat is available now