{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

How can the Altivar 58 drive be set to freewheel stop?

Issue:
Altivar 58 freewheel stop setup

Product Line:
Altivar 58

Environment:
All

Cause:
N/A

Resolution:
With ATV58 or Econoflex drives, freewheel stop is based on the status of a logic input. In the I-O menu (menu 5) set up a logic input to be freewheel stop (NST). When the input is at 0 state (when there is no voltage on the input), the drive will freewheel stop.
It is also possible to set the drive up to freewheel stop when the frequency goes below a preset value. In menu 3 (drc or drive menu) set Stt to NSt. Then set the FFt threshold in menu 2 (SEt or Adjust menu) to the desired frequency at which to begin freewheel stop.
See the keypad programming guide for more details.
 
Explore more

Can't find what you are looking for?

Reach out to our customer care team if you have any questions or need more technical support.
Explore more