Browse FAQs

What is the typical control circuit consumption at 24VDC for the U-Line LUB32?

Published date: 04 March 2020

Issue:
LUB32 consumption

Product Line:
Tesys U Motor Starters and Protectors

Environment:
n/a

Resolution:
The consumption depends on which control unit is installed into the Base unit. 
For a standard control unit inrush is 220mA and the sealed is 70mA.
For an advanced control unit inrush is 220mA and the sealed is 70mA.
For a multifunction control unit inrush is 200mA and the sealed is 75mA.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.