Browse FAQs

What is the difference between an FA36060 circuit breaker and an FAL36060?

Published date: 08 January 2020

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
FA style circuit breakers are designed for mounting into an I-Line panelboard, and they have plug-on connectors on the ``on`` side of the breaker and mechanical lugs on the ``off`` side. FAL style circuit breakers have mechanical lugs on both the ``on`` and ``off`` side, and they are designed for application as enclosed circuit breakers, or separately mounted applications.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.