Browse FAQs

What is the purpose of using output filter with an AC drive?

Published date: 17 June 2020

Issue:
AC drive output filter purpose.

Product Line:
Altivar drives

Environment:
All

Cause:
N/A

Resolution:
Output filters protect the motor in against The Reflective Wave Phenomenon and dV/dT Peak Voltages due to long motor lead length or high cable capacitance.
Additionally, the added inductance of a filter may help reduce motor heating, motor noise, and motor vibration.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.