Browse FAQs

What lugs come standard on the PowerPact H frame breaker?

Published date: 11 February 2020

Product Line:
Circuit Breakers

Environment:  
PowerPact H

Resolution:
The 15 A through 150 A breakers have the AL150HD lug that will accept wire sizes of #14 through 3/0 Al or Cu.  The lug kit comes with 3 lugs.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.