Browse FAQs

Are the CA2SK11UE7 and 31168-640-54 the same devices?

Published date: 26 June 2020

Issue:
Identify the difference between CA2SK11UE7 and 31168-640-54.

Product Line:
TeSys SK IEC stle relays

Environment:
TeSys SK IEC stle relays, Industrial Control Relays

Resolution:
Yes, these are the same components. CA2SK11UE7 is stocked in France and 31168-640-54 is stocked in North America (primarily used on class 8903 type L lighting contactors with form R6).
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.