Browse FAQs

Can a 9012GAR5 be used on water systems?

Published date: 06 July 2020

Issue:     
Is 9012GAR5  suitable to be used on water systems?

Product Line:
Pressure Switches and Pressure Sensors

Environment:
Pressure Switches - Square D™ NEMA

Resolution:
Yes, all components are compatible with water systems. However, salt water may attack standard flange material and may work best with 9013F Form Q. It is important to note that these switches are control rated devices. An interposing starter, or contactor must be used for switching a pump motor . Low level signals to PLCs or computers requires the use of an interposing low level switching relay.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.