Browse FAQs

What do the terms AC1 and AC3 mean?

Published date: 13 November 2018

Issue:
What are the utilization categories AC-1 and AC-3?

Product Line:
Schneider Electric Products

Environment:
Inductive and Resistive Loads

Resolution:
AC-1 - This category applies to all AC loads where the power factor is more than 0.95. These are primarily non-inductive or slightly inductive loads, such as resistive loads. Breaking the arc remains easy with minimal arcing and contact wear. 

AC-3 - This category applies to squirrel cage motors with breaking during normal running of the motor.
On closing, the contactor makes the inrush current, which is about 5 to 7 times the rated full load current of the motor.
On opening, the contactor breaks the rated full load current of the motor.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.