Browse FAQs

Is it possible to use TeSys GV2 and TeSys GV3 Range MPCB in DC applications?

Published date: 15 June 2020

The TeSys GV2 and TeSys GV3 range MPCB can be used in DC applications as per their technical specifications.

Refer the below wiring connection for TeSys GV range MPCB in DC network.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.