Browse FAQs

What type of 22 mm pushbuttons are used in Model 6 Motor Control Centers? Are incandescent or LED type lighted pushbuttons standard?

Published date: 23 June 2020

Issue:
22 mm pushbuttons used in Model 6 Motor Control Centers

Product Line:
Model 6 motor control centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
XB5/ZB5 type black plastic operators are normally installed for the 22 mm product offering. Incandescent lamps are standard, but LEDs are also an option.


CTA-ID : 2043517

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.