{}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Will it possible to see the multi core cable results beyond 240 or 300 mm2 from My Ecodial L.

For the Multi-core cable, software is showing the 240 or 300 mm2 conductor as a maximum cross sectional area result.
This restriction is due to the IEC standard. You can see from below reference;
But with My Ecodial L 3.4 it will be possible to pass besides this limitation during the software adaptation.
Moreover in many countries you can not find any multi core cable beyond 300 mm² CSA.

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.