Browse FAQs

What is the part number for the control card for the ATV312 drive?

Published date: 12 March 2020

Issue:
Looking for the  part number for the control card for the ATV312 drive?

Product Line:
Altivar ATV312

Environment:
All

Cause:
N/A

Resolution:
VW3A31201 is the input/output control card.  The package includes the control board which has the Input/Output screw terminal connections, RJ45 jack and a mounting screw. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.