Browse FAQs

How to change the default display to show something other than the output frequency on ATV12 and ATV312 drive?

Published date: 15 June 2020

Issue:
Change the value shown on the display for ATV12 and ATV312

Product Line:
ATV12, ATV312

Environment:
All models and serial numbers.

Cause:
None

Resolution:
To adjust the display so that other parameters can be viewed besides RFR, go to MON menu. Select a parameter and press and hold the enter key until the display blinks.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.