Browse FAQs

SoMove Lite v1.7.1.1 is it compatible with OS Operational System Windows 8?

Published date: 10 June 2020

Issue:
Is SoMove Lite v1.7.1.1 compatibility with OS Operational System Windows 8?

Product Line:
SoMove Software

Environment:
Version V1.7.1.1 on windows 8

Cause:
Drives Software compatibility with OS Windows 8.

Resolution:
No, From the SoMove Lite 1.7.1.1 Read Me file: 2.1 Supported Operating Systems
This software can be installed on the following operating systems:
Microsoft Windows XP Professional SP3 32 Bit
Microsoft Windows Vista Business Edition 32 Bit SP1
Microsoft Windows 7 32 bit Microsoft Windows 7/Vista 64 bit


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.