Browse FAQs

What is an E-19 error code on the ATV21/212 drive?

Published date: 14 May 2020

Issue:
 E-19 code on the ATV21/ATV212 drive.

Product line:
Altivar ATV21 ATV212

Environment:
All models, all serial numbers

Cause:
Drive trips with E-19 code.

Resolution:
E-19 error is a communication error between control CPUs on the ATV21/212 drive.  The fault is usually due to a loose connection on the cable connecting the control card and power board.  Another possible cause is that the power board or control board is damaged.  Make sure there is no 24V or 10V supply on VFD being shorted due to wiring.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.