{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

Is CMS 1000 Compatible with Windows 7 or Windows 8?

Issue:
Is CMS 1000 Powerlink AS software compatible with Windows 7 or 8 operation systems?

Product Line:
Powerlink AS

Environment:
Windows 7, Windows 8, Windows 10

Cause:
CMS1000 is an obsolete product and is not supported on Windows 7, 8,10

Resolution:
Run Windows XP mode in Windows 7 or Windows 8
 
Explore more

Can't find what you are looking for?

Reach out to our customer care team if you have any questions or need more technical support.
Explore more