Browse FAQs

What is the maximum Amp rating on the ATV312 +24Vdc terminal?

Published date: 30 June 2020

Issue:
ATV312 amperage available from the +24Vdc terminal

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
Customer use of the 24Vdc must not excede the rating for the power supply.

Resolution:
There is 100mA maximum available. Note that each logic input, LIx, requires 7mA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.