Browse FAQs

Can the ATV58 analog output be scaled?

Published date: 03 April 2020

Issue:
Request for analog output calibration

Product Line: 
ATV58

Environment
All

Cause
Adjustments

Resolution:  
The range is adjustable using the AOL and AOH parameters in the CtL menu.
The scaling is set by the specific assignment given to the analog output in the I-O menu.
Refer to the ATV58 keypad manual VVDED387047USR6/03 for specifics settings.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.