Browse FAQs

Why is the ATV61 with an water solution card resetting the R1 or R2 relay programming value after power cycle?

Published date: 04 March 2020

Issue:
ATV61 with Water Solutions card, losing the settings in R1 or R2 relay every time power is cycled to the drive.

Product Line:
Altivar ATV61

Environment:
All

Cause:
R1 or R2 will reset back to factory default after power cycle because its not part of the water solutions cards relays.  You can set it but it will always reset after you cycle power.

Resolution:
Don't use the Drives R1 and R2 relays when you have the water solutions card installed.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.