Browse FAQs

What is an INF7 fault on the ATV61 and ATV71 drives and how to remedy issue?

Published date: 10 June 2020

Issue:
INF7 fault on the ATV61 and ATV71 drives

Product Line:
Alitvar ATV61 and ATV71

Environment:
All

Cause:
Internal hard initialize fault

Resolution:
INF7 is a EEPROM initialization fault on the main control board of the VFD.  Attempt a full power cycle to clear fault.
If fault does not clear, VFD control board or the VFD itself may need to be replaced/repaired.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.