Browse FAQs

The green light on the ACE9XX communication module is permanently ON but the Sepam Series 20, 40 and 80 relay cannot communicate over the network.

Published date: 12 May 2020

Issue   
Trying to get communication to the Sepam relay over RS485.

Product Line
ACE959
ACE949(2)

Resolution
If the green led stays lit on the ACE9xx module that means there is a comms wiring issue. For normal working conditions, the green light would be:
a) turned off when Stand-By i.e. Commubnication frame to SCADA
b) flickering when communicating to SCADA


In order to fix the wiring issue, verify:

a) That the module is not grounded more than once. Often, the shield is exposed and grounded unnecessarily with the clamp, which is located below the terminals. Make sure that the shield isn't exposed and touching this clamp.


b) That the RS485 terminals are wired correctly. Here are the wiring diagrams for 2-wire and 4-wire communication:
For 2 wires:
Warning: L+ connects to L- and vise-versa when communicating to a powerlogic or third-party device on the same daisy chain!!!!


  • For 4 wire:

     
  •  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.