Browse FAQs

Is it possible to clear alarms and reset the SEPAM relay using the Logic Equation Editor or any other way?

Published date: 12 May 2020

Issue
User would like to know the options to clear alarms and/or reset SEPAM relay

Product Line
SEPAM series 20
SEPAM series 40
SEPAM series 60
SEPAM series 80

Resolution

SEPAM Series 20
The SEPAM Series 20 does not have the Logic Equation Editor, so therefore it isn't possible to create logic to clear alarms or reset the SEPAM Series 20. The only way of performing these functions in the Series 20 relay is using the Advanced UMI, SFT2841, or by sending commands via communications using PME or a third-party supervisory software.

SEPAM Series 40
The SEPAM Series 40 does have the Logic Equation Editor, but the user is unable to create logic to clear alarms or reset the SEPAM relay. The only output variables from "Circuit breaker control" that are available to the user are V_TRIPCB, V_CLOSECB and V_INHIBCLOSE. The only way the SEPAM Series 40 can clear alarms or reset the SEPAM relay is by using the Advanced UMI, SFT2841, or by sending a reset command via communications using PME or a third-party supervisory software.



SEPAM Series 60
The SEPAM Series 60 does have the Logic Equation Editor and the user is able to create logic to clear alarms or reset the SEPAM relay. When using the "Editor Assistance", the user will be able to use two separate logic functions "V_Clear" & "V_Reset" which can be programmed to perform these desired tasks. These functions can be very useful when the user is experiencing nuisance alarms and would like to frequently clear them and reset the relay. These functions can also be performed using the Advanced UMI, SFT2841, or by sending a reset command via communications using PME or a third-party supervisory software.




SEPAM Series 80
The SEPAM Series 80 does have the Logic Equation Editor and the user is able to create logic to clear alarms or reset the SEPAM relay. When using the "Editor Assistance", the user will be able to use two separate logic functions "V_Clear" & "V_Reset" which can be programmed to perform these desired tasks. These functions can be very useful when the user is experiencing nuisance alarms and would like to frequently clear them and reset the relay. These functions can also be performed using the Advanced UMI, SFT2841, or by sending a reset command via communications using PME or a third-party supervisory software.

Another way to clear alarms or reset the SEPAM series 80 relay is by use the Logipam function if this option is available in the Cartridge


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.