Browse FAQs

Why is the label for the SEPAM Series 80 printing vertically and not horizontally?

Published date: 12 May 2020

Issue    
The print label for the Sepam 80 is printing vertically not horizontally.

Product Line          
Sepam 80 Series

Resolution
The Sepam Series 80 with an Integrated UMI has a label running horizontally from left side to right side, but the Sepam Series 80 with Mimic-based UMI has a label running vertically from top to bottom. Therefore, the direction of the label depends on whether Advanced UMI or Mimic-based UMI is selected in SFT2841. If SFT2841 is printing the label vertically, then SFT2841 is configured to use a "Mimic-based UMI" model. In order to modify this setting so that the label prints horizontally, access SFT2841 "offline" or "online". Under the "Sepam hardware" tab, select "Integrated UMI" for the device model.

Once applied, click on Sepam -> Print label. This will print the label vertically.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.