Browse FAQs

What can SFT2841 be used for in a standard IEC61850 configuration?

Published date: 12 May 2020

Product Line   
SFT2841

Environment   
Software

Resolution   
STF2841 can be used for the following:
1. Get information from the SEPAM and ECI850 connected to the IEC61850 network. This can be done manually by keying the SEPAM description or automatically by using SFT2841 to poll the network to locate connected devices.
2. Extract ICD files from the library to build a configuration based on the SEPAM description.
3. Build a CID file as a result of the configuration for each SEPAM or ECI850 connected to the IEC61850 network. For an ECI850, it contains the configuration of all the SEPAM connected to the ECI850.
4. Generate an SCD file for use by other IEC61850 configuration tools. It contains the configuration of all SEPAM and ECI850 connected to the IEC61850 network.
5. Import a CID file into SFT2841 to modify it: for example to add or remove a SEPAM in the IEC61850 network topology.
6. Download a CID file into SEPAM or ECI850 with SFT2841.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.