Browse FAQs

Wrench 1 on the front display and the CCA634 module on a SEPAM is not recognized.

Published date: 13 May 2020

Issue           
Getting a wrench 1 on the front display and once connected with SFT2841 it has the CCA634 is missing.  The CCA634 is installed.

Product Line          
Sepam 20 Series
Sepam 40 Series
Sepam 80 Series

Resolution
This is due to the hardware on the SEPAM. In order to use a CCA634 the serial numbers below must be meet:
SEPAM 20 with serial number greater than 0301001
SEPAM 40 with serial number greater than 0623001
SEPAM 80 with serial number greater than 0629001
As a side note the CCA634 is not compatible with the following:
CSH30
CSH120
CSH200
ACE990
GO110


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.