Browse FAQs

Do the LPCT's require shorting before removal?

Published date: 13 May 2020

Issue                           
Need to run test on the Sepam and it has LPCTs.  Is it safe to run test on the Sepam or is a shorting block needed?

Product Line     
Sepam 
LPCT

Resolution
The LPCT's (Low power current transformers) do not require shorting before removal. The reason being is that they are a millivolt secondary.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.