Browse FAQs

What RTD's are supported with the SEPAM relays

Published date: 20 May 2020

Issue  
Need to know which RTD's are supported on the SEPAM relays.

Product Line  
SEPAM MET148-2

Resolution  
The SEPAM relays support the following three types of RTD's (this only applies to SEPAM relays that support the MET148-2 module):
1. PT100 (Platinum 100 ohm)
2. NI100 (Nickel 100 ohm)
3. NI120 (Nickel 120 ohm)

Note: The MET148-2 (RTD Module for the SEPAM relays) only supports three wire RTD's. This does not mean two wires and a shield.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.