Browse FAQs

May I use a standard Cat 5 or Cat 6 cable when connecting VAMP modules to the VAMP 221 or VAMP 321?

Published date: 20 May 2020

While a standard Cat 5 or Cat 6 cable will fit, it is not recommended to use with the VAMP relay due to the build of the cable. Standard cables do not have the necessary shielding or data through-put for reliable, fast detection and tripping times. Use only VAMP cables with the VAMP modules and master device.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.