Browse FAQs

What is the difference between L>ext and L>int on a VAMP 221 and VAMP 321?

Published date: 20 May 2020

The L>ext setting allows a slave device to initiate a trip from a condition outside its zone. The L>int setting allows a slave module to initiate a trip from a condition present in it's own zone.
Note: This does not affect how the master device will handle the condition as it is set at the master device level and not the slave module.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.