Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What is the difference between the 140XTS00206 and the 140XTS01206?
140-XTS-002-xx cable is rated for .5 Amps per point (read as point 5 Amps)
140-XTS-012-xx cable is rated for 2 Amps per point (read as 2 Amps)
The following table outlines the different Cablefast cables, their description, and rating:
140 XTS 002 03 3 foot cable with sub "D" connector Standard power .5 Amps
140 XTS 012 03 3 foot cable with sub "D" connector High power 2 Amps
140 XTS 002 06 6 foot cable with sub "D" connector Standard power .5 Amps
140 XTS 012 06 6 foot cable with sub "D" connector High power 2 Amps
140 XTS 002 09 9 foot cable with sub "D" connector Standard power .5 Amps
140 XTS 012 09 9 foot cable with sub "D" connector High power 2 Amps
140 XTS 002 12 12 foot cable with sub "D" connector Standard power .5 Amps
140 XTS 012 12 12 foot cable with sub "D" connector High power 2 Amps
140 XTS 102 06 6 foot cable with pigtail leads High power 2 Amps
140 XTS 102 15 15 foot cable with pigtail leads High power 2 Amps
R-82117
Note: the quantum line will be going obsolete 12/31/2018 and the M580 is the recommended replacement.
Did this answer your question?