Browse FAQs

Why do I receive the error message " Impossible to transfer project to PLC due to compatibility checks "?

Published date: 25 June 2020

Issue
When attempting to transfer a project to the PLC, the incompatibility message is returned.


Product line
Unity Pro, Control Expert

Resolution
The following are possible causes:

  • The selected CPU model from the program does not match the hardware.
  • The model matches, but the firmware version selected in the program is higher than the version in the hardware.
  • The program is using v1.xx firmware. (This is not always allowed with the most recent CPU firmwares)
  • Connected to the wrong PLC. (Try performing a read with no project open).
  • Multiple USB cables to different PLCs are connected. (Control Expert/Unity only supports one connection per PC)




 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.