Browse FAQs

What is the time-out value for the Advantys STB Ethernet NIM STBNIP2212 to go into a fallback state when communication to the Client is lost?

Published date: 10 September 2020

The time-out value is referred to as the Holdup Time. It is configured via the embedded web pages. Select the menu Configuration -> Client Controller. The value entered is in milliseconds ranging from 300ms-120000ms. A value of 0 is indefinite holdup time. Holdup time parameters are stored in Non-Volatile RAM.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.