Browse FAQs

What causes Concept error "Too many objects; it can't create more objects - AI-1336" ?

Published date: 15 May 2020

In most cases an export/re-import of the project using the Concept Converter (do not use the Re-connect to Equal mode)
will correct this error. If the project will not export due to analysing errors, try an export without exporting DFBs. This does not require a successful analysis.


Legacy KB System (APS) Data: RESL181493 V1.0, Originally authored by DaSo on 01/09/2007, Last Edited by DaSo on 01/09/2007
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.